Technical FAQs

Ask a Question

What are the watts loss for the ATS48D32Y soft starter?

The power dissipation in Watts is 25 W with Shorting/Bypass Contactor and 104 W without Shorting/Bypass Contactor.


CTA-ID : 2021527
Was this helpful?
What can we do to improve the information ?