Technical FAQs

Ask a Question

What size hubs are supplied with the Class 9421V1W30 or 9421V2W30 metallic enclosed vario switch?<br />

(1) 3/4`` NPT Meyers hubs is upplied in the top center and bottom center of the enclosure.


CTA-ID : 2022074
Was this helpful?
What can we do to improve the information ?