Technical FAQs

Ask a Question

What is the maximum number of mechanical operations of a ZB2 pushbutton.

Push buttons?3 million operations (Latching mushroom head push buttons: 300,000 operations. Illuminated selector
switches: 100,000 operations). The product life expressed is based on average usage and normal operating conditions.
Actual operating life will vary with conditions. The above statements are not intended to nor shall they create any express
or implied warranties as to product operation or life. For information on the limited warranty offered on this product,
please refer to Square D terms and conditions of sale found in the Square D Digest.

CTA-ID : 2026142
Was this helpful?
What can we do to improve the information ?