Technical FAQs

Ask a Question

Micrologic register 8716 for the Square D ID is reading 0. The value should be 15131. Should it be replaced?

This was a problem with the set-up of early trip units only. The trip unit needs to be replaced.

CTA-ID : 2021674
Was this helpful?
What can we do to improve the information ?