Technical FAQs

Ask a Question

Can a CU12L400L Meter main be fed from either side by the utility?

The utility section of this device has the largest knockout on the lower left, in the utility compartment. It should be fed only through the lower left of the utility compartment.


CTA-ID : 2021505
Was this helpful?
What can we do to improve the information ?