Technical FAQs

Ask a Question

Can a fuse lower than 30 ampere be used in a 30 ampere disconnect H361RB?

Issue:
Product Features

Product Line:
HD SS

Cause:
Fusing

Resolution:
Yes, as long as the fuse is a Class H, K, R or J and rated at 600Vac, and rated 30A or less.


CTA-ID : 2021501
Was this helpful?
What can we do to improve the information ?