Technical FAQs

Ask a Question

Can a main breaker be installed in an HOM48L125GC load center?

That type of load center is main lug only, and is not convertible to main breaker with a standard main breaker type. However, a branch breaker can be backfed and used as a main, using an HOM1RK mounting kit. This branch breaker used as a backfed main will take up two branch spaces.

CTA-ID : 2021498
Was this helpful?
What can we do to improve the information ?