Technical FAQs

Ask a Question

Is there a NEMA 1 enclosure available for a 1200A breaker?

There is not specifically a NEMA 1 unit available. However, the NEMA 12/3R/5 rated NA1200AWK can be used in applications where a NEMA 1 enclosure is needed.


CTA-ID : 2021497
Was this helpful?
What can we do to improve the information ?