Technical FAQs

Ask a Question

Is the a Cable Operating Mechanism for NSF or NSJ Circuit Breakers?

Yes, as outlined below: (Note: Kits DO NOT include handle operator, Class 9422 Type A handles must be order separately)

NSF - 3 Pole:
9422CSF30 - 36 inch cable length.
9422CSF50 - 60 inch cable length.
9422CSF70 - 84 inch cable length.
9422CSF10 - 120 inch cable length.

NSF - 4 Pole:
9422CSF304 - 36 inch cable length.
9422CSF504 - 60 inch cable length.
9422CSF104 - 120 inch cable length.

NSJ - 3 Pole:
9422CSJ30 - 36 inch cable length.
9422CSJ50 - 60 inch cable length.
9422CSJ10 - 120 inch cable length.

NSJ - 4 Pole:
9422CSJ304 - 36 inch cable length.
9422CSJ504 - 60 inch cable length.
9422CSJ104 - 120 inch cable length.


CTA-ID : 2021314
Was this helpful?
What can we do to improve the information ?