Technical FAQs

Ask a Question

Can I use two QOTHPA handle lockoffs to lockoff both handles of a tandem breaker?

It is not necessary to mount two QOTHPA units, since one QOTHPA will lock off both handles of the tandem breaker. It will lock both handles either on or off.


CTA-ID : 2021922
Was this helpful?
What can we do to improve the information ?