Technical FAQs

Ask a Question

What is the catalog number for the handle padlock attachment for an IL or ILL breaker, such as IL34400?

Issue:
What is the catalog number for the handle padlock attachment for an IL or ILL breaker?

Product Line:
Legacy Circuit Breakers

Environment:
Electrical Distribution Equipment

Cause:
Need to be able to lock the IL frame breaker in the ON or OFF position.

Resolution:
Use padlock attachment HPALM to lock in the ON or OFF position.
Was this helpful?
What can we do to improve the information ?