Technical FAQs

Ask a Question

What is the 400 amp, 3 pole , plug-in unit for the SD1341 busway?

Issue:
What is the 400 amp, 3 pole , plug-in unit for the SD1341 busway?

Product Line:
Busway

Environment:
APD and SD Busway

Cause:
Maintenance

Resolution:
SD67446. This is a circuit breaker plug-in unit. Fusible plug-in units for this style of busway are no longer available. Refer to page 10-11 Digest 173 for other circuit breaker plug-in units available for the APD and SD Busway.


CTA-ID : 2021028
Was this helpful?
What can we do to improve the information ?