Technical FAQs

Ask a Question

What part is available to run a #4 CU ground wire from a HOM load center neutral assembly or ground bar to a ground rod ?

The terminals on the Neutral and the Ground Bar will accept a #14 to #4 copper wire. If a larger lug is needed use a field installable lug LK70AN

CTA-ID : 2021026
Was this helpful?
What can we do to improve the information ?