Technical FAQs

Ask a Question

Is external control power required for control voltage with the enclosed 8638 and 8639 ATS48 softstarter?

No.  115Vac Control Power Transformer (CPT) is included as standard. This provides power to operate the included control relays and contactors and the control power for the soft starter.

CTA-ID : 2020831
Was this helpful?
What can we do to improve the information ?