Technical FAQs

Ask a Question

Can base channels be provided on a NEMA 4/4X stainless steel panelboard enclosure?

Issue:
Can base channels be provided on a NEMA 4/4X stainless steel panelboard  enclosure?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Panelboard enclosures sold and supported in the USA.

Cause:
Are base channels available for stainless steel enclosures?
 
Resolution:
Base channels can be provided on a NEMA 4/4X stainless steel enclosure as a special. Contact Peru TAG or your local Schneider Sales Office  for pricing details










CTA-ID : 2020818
Was this helpful?
What can we do to improve the information ?