Technical FAQs

Ask a Question

How many lead wire are attached to the FA/FH/FC/FI breaker with a suffix of ``1352``?

Six lead wires. Two yellow wires (A contacts - NO), two blue wires (B contacts - NC), and two striped wires (common).


CTA-ID : 2020555
Was this helpful?
What can we do to improve the information ?