Technical FAQs

Ask a Question

Why don`t we make a 240 volt not fusible safety switch?

Fuses are manufactured for 240 volts or 600 volts applications, Since the same fuse clip cannot accept both ratings we offer fusible switches in 240 or 600 volts. Since Non fusible safety switches do not require fuses, the 600 volt switches can be used for voltages up to 600 volts. This makes selection easier and keeps prices lower by consolidation of the product offering


CTA-ID : 2020549
Was this helpful?
What can we do to improve the information ?