Technical FAQs

Ask a Question

What frame size Main Breaker is used for the QO13040L200G load center?

Issue:
Product Design Features

Product Line:
QO Single Phase Load Centers

Environment:
Main Circuit Breaker

Cause:
Application

Resolution:
The QO13040L200G Convertible Mains load centers uses the QOM2 Frame Size and the below catalog numbers and amperages are available for the QOM2 frame.
100amp = QOM2100VH
125amp = QOM2125VH
150amp = QOM2150VH
175amp = QOM2175VH
200amp = QOM2200VH
225amp = QOM2225VH( this can ONLY be used in the load center is Rated up to 225amp MAX.)


CTA-ID : 2020547
Was this helpful?
What can we do to improve the information ?