Technical FAQs

Ask a Question

What tenant breaker is used with the EZMK.... branch devices?

a 400amp DJM type. The breaker is factory installed and field adjustable from 160A to 400A.


CTA-ID : 2021231
Was this helpful?
What can we do to improve the information ?