Technical FAQs

Ask a Question

Why does the ATV58 indicate in menu 5 that have LI5, LI6 and other additional I/O that would be on the Analog I/O card when the card installed is the GPO yet it does not show any additonal Analog Outputs?

With the GPO card installed the additional terminal designation are not identified in menu 5.
The LI5 & LI6 assignments are shown in menu 5 but are not programmable. Be sure to set LI5 & LI6 to no:not assigned.
To program the AO1, AO2 & AO3 of the GPO card, go into menu 8 and set them up according to Bulletin No. 300072-450-03.

CTA-ID : 2021003
Was this helpful?
What can we do to improve the information ?