Technical FAQs

Ask a Question

Are lugs for use on Low Voltage Transformers by SquareD/Schneider Electric acceptable for use with 75 degree C wire?

Issue:
Wiring of Low Voltage Transformers

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Wire ampacity at 90C and 75C

Resolution:

Compliance with UL and the NEC requires using 90 degree C wire rated for a 75 degree C wire ampacity.



CTA-ID : 2020805
Was this helpful?
What can we do to improve the information ?