Technical FAQs

Ask a Question

Can a 9065 Motor Logic solid state overload be used on 400 hertz?

No. The frequency limit is between 50 and 60 hertz.


CTA-ID : 2020779
Was this helpful?
What can we do to improve the information ?