Technical FAQs

Ask a Question

What gauge steel is used in the construction of a Model 6 LVMCC section?

Corner Channels - 12 Ga.
Back Plate 20 thru 30 in. wide - 16 Ga.
Back Plate 35 in. wide - 14 Ga.
End Closing Plates - 16 Ga. (NEMA 3R - 12 Ga.)
Unit Doors - 14 & 16 Ga. (NEMA 3R - 12 Ga. on outer door)
Side Channels - 11 Ga.
Top & Bottom Frame - 12 Ga.
Top & Bottom Plates - 14 Ga.
Base Channels - 10 Ga.
Lifting Angle - 7 Ga.

Also see document link to the Model 6 Motor Control Center Catalog pg. 13.


CTA-ID : 2025225
Was this helpful?
What can we do to improve the information ?