Technical FAQs

Ask a Question

What is the replacement diaphragm actuator for the 9012 GEW1, 21 pressure switch?

9998PC177. See Digest 173, page 20-10. Note the star footnote which is explained in detail at the bottom of the page. Some forms of the switch require modification of the diaphram and its mounting mechanism., those forms are listed in the two tables on page 20-11.


CTA-ID : 2020528
Was this helpful?
What can we do to improve the information ?