Technical FAQs

Ask a Question

Can the LA9P307 Profibus DP/Modbus Gateway device be used with Altivar 31 drives?

This is not the recommended device for this application.  This device is not recommended for use in the United States and we do not support or offer literature on it. We recommend use of the LUFP7 Profibus DP/Modbus gateway device.  The LA9P307 was listed in some US Drives literature by mistake.

Reviewed 7/2011

CTA-ID : 2020514
Was this helpful?
What can we do to improve the information ?