Technical FAQs

Ask a Question

Want is the part number for the remote mount keypad for the ATV31?

VW3A31101.
This kit includes a remote keypad, remote mount hardware seal and screws for IP65 mounting on enclosure door and 3 meter cable fitted with 2 connectors.


CTA-ID : 2021208
Was this helpful?
What can we do to improve the information ?