Technical FAQs

Ask a Question

What materials are needed for mounting a NQOD430L100CU in a MH35 box instead of the standard MH29 ? <br /> <br />

(1) 80110-290-02 deadfront extension
(2) 80110-288-02 6`` rail extension
(4) 21590-17081 screws
(1) MHC35F/S cover
to be mounted on mains end


CTA-ID : 2020991
Was this helpful?
What can we do to improve the information ?