Technical FAQs

Ask a Question

Why does the ATV58 drive not start, even though it has speed reference along with good voltage on its forward run and freewheel stop terminals, until the RUN button is pushed on the keypad?

This indicates the drive is in keypad command mode. In order to start it from the terminal strip you will have to go to menu 4, and set the LCC parameter to NO.

CTA-ID : 2020989
Was this helpful?
What can we do to improve the information ?