Technical FAQs

Ask a Question

What type and size wire should supply the cell switch on an NW cradle?

Cell Switch Wiring: Shielded pair cable or twisted pair copper wires: #22 to#16 AWG (0.5 to 1.25 mm^2)


CTA-ID : 2020988
Was this helpful?
What can we do to improve the information ?