Technical FAQs

Ask a Question

What type and size wire should supply the CCM S48377 with its 24 Vdc power?

Power Cable: Shielded pair cable or twisted pair copper wires: #16 to #12 AWG (1.5 to 3 mm^2), color-coded red and black

CTA-ID : 2020987
Was this helpful?
What can we do to improve the information ?