Technical FAQs

Ask a Question

What is the recommended wire size and type for modbus communications wiring the for Powerpact and NW breakers?

Issue:
What is the recommended wire size and type for modbus communication wiring the for Powerpact and NW breakers?

Product Line:
Powerpact and Masterpact

Environment:
Electrical Distribution

Cause:
Communications needs wires

Resolution:
Bulletin 0613IB1201 says to use #22 AWG Belden® shielded / twisted cable (8723) for communication wiring.

CCM S48377
Was this helpful?
What can we do to improve the information ?