Technical FAQs

Ask a Question

Does Square D offer a 3 pole, 30 amp, 480 Vac rated breaker for DIN rail mounting?

 

Issue:

Does Square D offer a 3 pole, 30 amp, 480 Vac rated breaker for DIN rail mounting?

 

Product Line:

Powerpact H and J

 

Environment:

Distribution

 

Cause:

Mounting

 

Resolution:

Yes. You may use the Power pact H-Frame with a DIN rail mounting kit. Catalog # S29305

Yes, Powerpact H & J frame 3-pole breakers can be DIN rail mounted. Use kit # S29305.  
DIN rail mounting kit (requires 15 mm depth on a 35 mm DIN rail)
Fits 3 pole module breakers only. (Not available in 2 pole)

See instruction bulletin, 48940-239-01.

CTA-ID : 2020498

Was this helpful?
What can we do to improve the information ?