Technical FAQs

Ask a Question

Is the 9037HG float switch a two pole device?

Iit is indeed a two pole device. It can be used on a 3 phase circuit by wiring each of 2 phases thru the switch, and wiring the third directly to the motor. In this case, use a 3 phase disconnect upstream of the switch.

CTA-ID : 2020497
Was this helpful?
What can we do to improve the information ?