Technical FAQs

Ask a Question

What is the replacement door latch for the OLD cover QOC30F?

Issue:
Previous Design repair parts

Product Line:
QO Load Centers

Environment:
Repair parts

Cause:
maintenance

Resolution:
The QOC30F is a very old cover and it did not contain an actual 'Door Latch', BUT contained a Pull ring part# 186012 and Spring part# 163471. BUT THESE ARE BOTH OBSOLETE AND NO LONGER AVAILABLE. Also, the cover itself is Obsolete and no longer available with NO replacement.


CTA-ID : 2021198
Was this helpful?
What can we do to improve the information ?