Technical FAQs

Ask a Question

Do the hard wired surge arresters meet the OWHX requirements?

Yes, this listing covers surge arresters intended to afford protection against surge related damage to secondary distribution wiring systems and/or to equipment connected thereto. Includes one of the following names, Surge Arrester, Secondary Surge Arrester, Secondary MOV Surge Arrester, Secondary Metal-Oxide Surge Arrester, Secondary Valve Type Arrester.
ADDED BY SURGE ARRESTER FACILITY
OWHX is UL`s designator code for all Secondary Surge Arrester products. There is another code, XUHT, for all TVSS products. The SDSA products are both listed under UL`s Secondary Surge Arrester standard aka OWHX. These designator codes are not referenced on product labels or literature but is referenced on all of our UL listing documents.


CTA-ID : 2020744
Was this helpful?
What can we do to improve the information ?