Technical FAQs

Ask a Question

What are the dimensions for the 250, 300, 350, 400, 450, or 500 HP 8839 ATV58M enclosed drive with bypass?

The dimensions in the manual only list the Pre-engineered units. The 250 hp and above are not included.
Contact Seneca for dimensions of the units that are not Pre-engineered or shown in the catalog or user`s guides.


CTA-ID : 2020480
Was this helpful?
What can we do to improve the information ?