Technical FAQs

Ask a Question

Is there a password to protect parameters in the ATV31 drive?

Yes.
In the SUP menu, the COd parameter can be used to enter a numerical code that restricts access to adjustment parameters in the drive.  Only the display parameters are accessible, with only a temporary choice of the parameter displayed.

Reviewed 6/2011


CTA-ID : 2021186
Was this helpful?
What can we do to improve the information ?