Technical FAQs

Ask a Question

Need to know if our drives are NAFTA approved so can determine if Tarrif Free for shipping out of the country.

The drives are not NAFTA approved which would require the majority of components or certain components to have been manufactured in America.

CTA-ID : 2021182
Was this helpful?
What can we do to improve the information ?