Technical FAQs

Ask a Question

What are the repair parts for a RC2M200SH Series M01?

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4056206950
Main Breaker Section Cover Assembly - 4053449250
Main Breaker Section Cover Hinges - (2) X2983
Main Breaker Section Cover Hinge Mounting Screws - (2) 2159414081
Dead Front Interior Trim - 4053443801
Dead Front Interior Trim Mounting Screw - 4020513001K ( This kit contains 10 screws, but only one screw is required to secure the trim)
Dead Front Interior Trim Filler Plates - (2) QOFP
Meter Base Assembly - 4056250250 (Includes meter base, (2) line side lugs, (4) meter jaws and (4) meter jaw blade guides, (2) load side lugs (feeds QO base), load side bussing (feeds QOM2-VH) and (4) horn bypass)
Meter Jaw - (4) 4052706950 (OBSOLETE - REPLACED BY 7329794850)
Meter Jaw Mounting Nuts - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Left Line Side Lug Assembly - 4056207850
Right Line Side Lug Assembly - 4056207950
Horn Bypass - (4) 4056150901
Fifth Jaw Kit - 5J
Closing Cap - (2) ACP
Main Breaker - QOM2-VH type, 200A maximum
Main Breaker (QOM2-VH) Mounting Nuts - (2) 2342702001
Main Breaker - QO-VH type, 50A maximum
Main Breaker (QO-VH) Mounting Base - 4050443650, Mounting Screw 2196617201
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE


CTA-ID : 2005849
Was this helpful?
What can we do to improve the information ?