Technical FAQs

Ask a Question

What is the UL suffix meaning in reference to DZ5 cable ends?

Suffix UL was used to indicate that the unit was component recognized provided the AT1PA2 crimp tool was used.
The ``UL `` suffix is no longer needed for the DZ5 cable ends, but still are UL Recognized as component parts with regards to using the AT1PA2 tool.

CTA-ID : 2020732
Was this helpful?
What can we do to improve the information ?