Technical FAQs

Ask a Question

What is the coil consumption for a LC1F150?

For an AC 60 hertz coil the inrush is 660 VA and the sealed is 55 VA.
For an AC 50 hertz coil the inrush is 550 VA and the sealed is 45 VA.
For a DC coil the inrush is 560 watts and the sealed is 4.5 watts.


CTA-ID : 2020726
Was this helpful?
What can we do to improve the information ?