Technical FAQs

Ask a Question

What are replacement hinges for an old QO NEMA 1(indoor) load center cover?

Issue:
Design repair parts

Product Line:
QO Load centers

Environment:
Repair parts

Cause:
maintenancve

Resolution:
Use part number 4028356450K. This hinge kit contains one old style and one new style hinge (choose the one needed and discard the other). Only one hinge can be repaired with this kit. Order the appropriate number of kits to repair the number of hinges needing repair.


CTA-ID : 8114
Was this helpful?
What can we do to improve the information ?