Technical FAQs

Ask a Question

Can I use multiple partitions in wall duct to divide the duct into two or three compartments?

Yes - use partition RWTP60. These are 5 feet long.
Also, if three compartment division is needed in Tees and Crosses, use the following dividers:
Tees - RWT10PTE or RWT18PTE
Crosses - RWT10PXE or RWT18PTE


CTA-ID : 2020452
Was this helpful?
What can we do to improve the information ?