Technical FAQs

Ask a Question

What is the warranty period on a SDSB1175C Surgebreaker plus?

The warranty shall be in effect three (3) years following the date of purchase of the Surgebreaker Plus device, except that when the Surgebreaker Plus device is used in conjunction with both a point of use surge protective device and a QO or Homeline Load Center device, then this warranty shall be in effect for five (5) years following the date of purchase of the Surgebreaker Plus device.


CTA-ID : 2020418
Was this helpful?
What can we do to improve the information ?