Technical FAQs

Ask a Question

Can the Altivar 28 drive be stopped using the terminal controls if the local operator kit (VW3A28100) is installed on the drive?

Yes. The stop inputs are still active after the local operator kit is installed.
Program a logic input (LI2, LI3 or LI4) for Freewheel (nSt) or Fast Stop (FSt).
Wire a stop circuit between +24 and the logic input to open for a stop command and to close to allow the drive to run.


CTA-ID : 2019412
Was this helpful?
What can we do to improve the information ?