Technical FAQs

Ask a Question

What is the recommended potentiometer size on ATV31 drive?

The 10 VDC power supply and the analog input of the Altivar 31 drive can operate with any potentiometer from 1k to 10k ohms.

Reviewed 6/2011

CTA-ID : 2019252
Was this helpful?
What can we do to improve the information ?