Technical FAQs

Ask a Question

What is the UL file number for the ATV31?

UL File number E164874 CCN NMMS is correct.
The file E164874 CCN NMMS lists the ATV66 and ATTV68 on the UL site. As of November 2004, the ATV31 is not shown on the UL website.
This is the same file that all of the Altivar Family of drives are listed under. The file number does not change but, the newer drive part numbers are added to the file.
See also, NMMS.E116875
NOTE: Some of the attachment links contain a documents that are not for general distribution.
For details, contact Drive Products Support at 888-SQUARED or E-mail drive.products.support@us.schneider-electric.com


CTA-ID : 2019189
Was this helpful?
What can we do to improve the information ?