Technical FAQs

Ask a Question

Can I replace the 100A main breaker in a QO327M100 load center? I would like to install a 70A main breaker. What is the catalog number of the new breaker?

The main breaker in that panel is a QO3100VH. You could replace it with a QO370VH breaker. If ordering large quantities of these panels, the 70A main breaker can be factory installed.


CTA-ID : 2021147
Was this helpful?
What can we do to improve the information ?