Technical FAQs

Ask a Question

Pls adv. if we can supply internal TVSS unit with a temp.<br />range or +85 Deg. C.

Surgelogic TVSS is limited on the high end of temperature ratings to +65 degrees C.
That is quite warm, 149 degrees F, and I wonder if the gear where it would be applied can exceed that temperature.


CTA-ID : 2021141
Was this helpful?
What can we do to improve the information ?