Technical FAQs

Ask a Question

I have EZM metering with three phase main device and three phase branches. Can I install a single phase main device to feed the three phase branches if my service changes to single phase?

No. It is not permissible to feed a three phase branch with a single phase main device. The UL listing and labeling of the equipment are issues.

CTA-ID : 2021139
Was this helpful?
What can we do to improve the information ?